:CMODe:CRECovery:SOPLl:OJTF:LBANdwidth

Command Syntax

:CMODeN:CRECovery:SOPLl:OJTF:LBANdwidth <loop_bandwidth>
            

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<loop_bandwidth> is a double.

Query Syntax

:CMODeN:CRECovery:SOPLl:OJTF:LBANdwidth?

Description

Specifies the PLL's loop bandwidth (also known as the -3 dB BW).

Example Command Sequence

:CMODe1:CRECovery:MODE SOPLl
:CMODe1:CRECovery:PLL:MODE OJTF
:CMODe1:CRECovery:SOPLl:OJTF:LBANdwidth 1.779E+6
:CMODe1:CRECovery:SOPLl:OJTF:DFACtor 0.707