:CMODe:CRECovery:SRATe

Command Syntax

:CMODeN:CRECovery:SRATe <symbol_rate>
            

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<symbol_rate> is a double.

Query Syntax

:CMODeN:CRECovery:SRATe?

Description

Sets the common-mode waveform N Symbol Rate for clock recovery. This is the baud rate associated with the input waveform.

Example Command Sequence

:CMODe1:CRECovery:MODE CFRequency
:CMODe1:CRECovery:SRATe 2.97E+09
:CMODe1:CRECovery:CFRequency:MODE SAUTomatic