:CMODe:CRECovery:TOPLl:PFReq
Command Syntax
:CMODeN:CRECovery:TOPLl:PFReq <pole_frequency>
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
<pole_frequency> is a double.
Query Syntax
:CMODeN:CRECovery:TOPLl:PFReq?
Description
Specifies the third-order PLL's pole frequency, ωp, which is an angular frequency in radians/sec. ω is equivalent to 2πf, where f is frequency in Hertz.
Example Command Sequence
:CMODe1:CRECovery:MODE TOPLl :CMODe1:CRECovery:TOPLl:PFReq 4.714E+06