:CMODe:CRECovery:TOPLl:DFACtor

Command Syntax

:CMODeN:CRECovery:TOPLl:DFACtor <damping_factor>
            

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<damping_factor> is a double.

Query Syntax

:CMODeN:CRECovery:TOPLl:DFACtor?

Description

Specifies the third-order PLL's damping factor (ΞΆ).

Example Command Sequence

:CMODe1:CRECovery:MODE TOPLl
:CMODe1:CRECovery:TOPLl:DFACtor 1.0