:CMODe:CRECovery:ECLock:CFRequency
Command Syntax
:CMODeN:CRECovery:ECLock:CFRequency <frequency>
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
<frequency> is a real number used for the clock frequency of the PLL.
Query Syntax
:CMODeN:CRECovery:ECLock:CFRequency?
Description
With the Explicit 1st or 2nd Order PLL clock recovery methods (see :CMODe:CRECovery:MODE), this command specifies the clock frequency of the PLL.
Example Command Sequence
:CMODe1:CRECovery:MODE EFOPll :CMODe1:CRECovery:ECLock:CFRequency 1.485E+09