:CMODe:CRECovery:PLL:ICCount
Command Syntax
:CMODeN:CRECovery:PLL:ICCount <idle_clock_count>
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
<idle_clock_count> is an integer from 10 to 200.
Query Syntax
:CMODeN:CRECovery:PLL:ICCount?
Description
Specifies the number of clock periods without a data transition (edge) that indicate an idle condition. This option lets protocol decoders suppress decode for idle data periods on serial data links that go quiescent for a period of time and then restart transmitting.
Example Command Sequence
:CMODe1:CRECovery:MODE FOPLl :CMODe1:CRECovery:PLL:ICCount 80