:DIFF:CRECovery:CSRate?
:DIFF CRECovery Commands
- :DIFF CRECovery Commands
- :DIFF:CRECovery:CEALgorithm
- :DIFF:CRECovery:CEIDle
- :DIFF:CRECovery:CFRequency:EDIRection
- :DIFF:CRECovery:CFRequency:MODE
- :DIFF:CRECovery:CSRate?
- :DIFF:CRECovery:DDRFive:CAFLatency
- :DIFF:CRECovery:DDRFive:CAFSource
- :DIFF:CRECovery:DDRFive:DQSSource
- :DIFF:CRECovery:DDRFive:POLength
- :DIFF:CRECovery:DDRFive:PRLength
- :DIFF:CRECovery:DDRFive:RWMode
- :DIFF:CRECovery:DDRFive:STDDelay
- :DIFF:CRECovery:DREMoval
- :DIFF:CRECovery:ECLock:ALIGn
- :DIFF:CRECovery:ECLock:CFRequency
- :DIFF:CRECovery:ECLock:CMULtiplier
- :DIFF:CRECovery:ECLock:DELay
- :DIFF:CRECovery:ECLock:EDIRection
- :DIFF:CRECovery:ECLock:SOURce
- :DIFF:CRECovery:FOPLl:LBANdwidth
- :DIFF:CRECovery:FOPLl:LBDivisor
- :DIFF:CRECovery:FSRate
- :DIFF:CRECovery:ICCount
- :DIFF:CRECovery:MODE
- :DIFF:CRECovery:PLL:EDIRection
- :DIFF:CRECovery:PLL:MODE
- :DIFF:CRECovery:PLL:SSCCorrect
- :DIFF:CRECovery:PLL:SSPercent
- :DIFF:CRECovery:PLL:SSType
- :DIFF:CRECovery:PLL:STIMe
- :DIFF:CRECovery:PLL:TDEPendent
- :DIFF:CRECovery:PRESets
- :DIFF:CRECovery:PRESets:SELections?
- :DIFF:CRECovery:SOPLl:JTF:LBANdwidth
- :DIFF:CRECovery:SOPLl:JTF:LBDivisor
- :DIFF:CRECovery:SOPLl:JTF:PEAKing
- :DIFF:CRECovery:SOPLl:OJTF:DFACtor
- :DIFF:CRECovery:SOPLl:OJTF:LBANdwidth
- :DIFF:CRECovery:SOPLl:OJTF:LBDivisor
- :DIFF:CRECovery:SRATe
- :DIFF:CRECovery:SRATe:STATus?
- :DIFF:CRECovery:SRATe:STATus:DETails?
- :DIFF:CRECovery:SRATe:STATus:REASon?
- :DIFF:CRECovery:TOPLl:DFACtor
- :DIFF:CRECovery:TOPLl:NFReq
- :DIFF:CRECovery:TOPLl:PFReq
- :DIFF:CRECovery:TRACking
- :DIFF:CRECovery:ZOPLl:LFPole
- :DIFF:CRECovery:ZOPLl:PPOLe
- :DIFF:CRECovery:ZOPLl:SPOLe
Query Syntax
:DIFFN:CRECovery:CSRate?
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Description
Returns the computed symbol rate that is used to scale a real-time eye.
If you turn on a real-time eye or anything that requires clock recovery, the computed symbol rate is set.