:DIFF:CRECovery:SRATe
Command Syntax
:DIFFN:CRECovery:SRATe <symbol_rate>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<symbol_rate> is a double.
Query Syntax
:DIFFN:CRECovery:SRATe?
Description
Sets the differential waveform N Symbol Rate for clock recovery. This is the baud rate associated with the input waveform.
Example Command Sequence
:DIFF1:CRECovery:MODE CFRequency :DIFF1:CRECovery:SRATe 2.97E+09 :DIFF1:CRECovery:CFRequency:MODE SAUTomatic