:DIFF:CRECovery:PLL:SSPercent
Command Syntax
:DIFFN:CRECovery:PLL:SSPercent <percent>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<percent> is a double.
Query Syntax
:DIFFN:CRECovery:PLL:SSPercent?
Description
When the application of SSC (spread-spectrum clocking) correction is enabled (see :DIFF:CRECovery:PLL:SSCCorrect), this command specifies the magnitude of the symbol rate change (spread) as a percent.