:DIFF:CRECovery:ZOPLl:SPOLe
Command Syntax
:DIFFN:CRECovery:ZOPLl:SPOLe <secondary_pole_frequency>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<secondary_pole_frequency> is a double.
Query Syntax
:DIFFN:CRECovery:ZOPLl:SPOLe?
Description
Specifies the fifth-order PLL's secondary pole frequency, ω1, which is an angular frequency in radians/sec. ω is equivalent to 2πf, where f is frequency in Hertz.
Example Command Sequence
:DIFF1:CRECovery:MODE ZOPLl :DIFF1:CRECovery:ZOPLl:SPOLe 24.38E+06