:DIFF:CRECovery:TRACking
Command Syntax
:DIFFN:CRECovery:TRACking {ON | OFF | 1 | 0}
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:CRECovery:TRACking?
Query Response
{1 | 0}
Description
Specifies whether the differential waveform's clock recoverysettings should track (use) the global settings or use custom settings specific to this waveform.
When using the global settings, see :CRECovery Subsystem commands.
When using custom settings specific to this real-time eye, see :DIFF CRECovery Commands.