:DIFF:CRECovery:SOPLl:JTF:PEAKing
Command Syntax
:DIFFN:CRECovery:SOPLl:JTF:PEAKing <peaking_in_dB>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<peaking_in_dB> is a double.
Query Syntax
:DIFFN:CRECovery:SOPLl:JTF:PEAKing?
Description
When specifying the PLL's loop bandwidth in terms of the JTF 3 dB BW, you also need to specify the peaking of the JTF.
Example Command Sequence
:DIFF1:CRECovery:MODE SOPLl :DIFF1:CRECovery:PLL:MODE JTF :DIFF1:CRECovery:SOPLl:JTF:LBDivisor 1.047E+3 :DIFF1:CRECovery:SOPLl:JTF:PEAKing 1.25