:DIFF:CRECovery:SRATe:STATus:REASon?

Query Syntax

:DIFFN:CRECovery:SRATe:STATus:REASon?

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :DIFF:CRECovery:SRATe measurement. If the measurement was successful, a null string is returned.

Use the :DIFF:CRECovery:SRATe:STATus? parent query to determine if the measurement has failed.

See Also