:DIFF:CRECovery:DDRFive:PRLength
Command Syntax
:DIFFN:CRECovery:DDRFive:PRLength <#_of_tCK>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<#_of_tCK> is an integer.
Query Syntax
:DIFFN:CRECovery:DDRFive:PRLength?
Description
When an DDR5 clock recovery mode is selected (see :DIFF:CRECovery:MODE), this command specifies the preamble length used in the device under test (DUT) for the selected burst type (see :DIFF:CRECovery:DDRFive:RWMode).