:DIFF:CRECovery:SOPLl:OJTF:LBDivisor
Command Syntax
:DIFFN:CRECovery:SOPLl:OJTF:LBDivisor <loop_bandwidth_divisor>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<loop_bandwidth_divisor> is a double.
Query Syntax
:DIFFN:CRECovery:SOPLl:OJTF:LBDivisor?
Description
Specifies a number that the symbol rate is divided by to get the loop bandwidth.
Example Command Sequence
:DIFF1:CRECovery:MODE SOPLl :DIFF1:CRECovery:PLL:MODE OJTF :DIFF1:CRECovery:SOPLl:OJTF:LBDivisor 1.670E+3 :DIFF1:CRECovery:SOPLl:OJTF:DFACtor 0.707