:DIFF:CRECovery:SRATe:STATus:DETails?

Query Syntax

:DIFFN:CRECovery:SRATe:STATus:DETails?

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

If the status of the clock recovery symbol rate is questionable or invalid (see :DIFF:CRECovery:SRATe:STATus?), this query returns a string that may provide additional details.

If the status of the clock recovery symbol rate is valid, this query returns an empty string.

For a basic reason for the questionable or invalid status, use the :DIFF:CRECovery:SRATe:STATus:REASon? sibling query.

See Also