:DIFF:CRECovery:FOPLl:LBANdwidth
Command Syntax
:DIFFN:CRECovery:FOPLl:LBANdwidth <loop_bandwidth>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<loop_bandwidth> is a double.
Query Syntax
:DIFFN:CRECovery:FOPLl:LBANdwidth?
Description
Specifies the PLL's loop bandwidth (also known as the -3 dB BW).
Example Command Sequence
:DIFF1:CRECovery:MODE FOPLl :DIFF1:CRECovery:FOPLl:LBANdwidth 1.782E+6