:DISPlay:BWRap

Command Syntax

:DISPlay:BWRap  {ON | OFF | 1 | 0}

Query Syntax

:DISPlay:BWRap?

Query Response

{1 | 0}

Description

Enables or disables the wrapping of badges at the bottom of the display.

When badges are wrapped, you no longer have to scroll left or right to view the badges that cannot fit in the available viewing area.

Note that you can also use the :DISPlay:BLAYout command to specify compact or full-height badges.