:DISPlay:GSSPectrum

Command Syntax

:DISPlay:GSSPectrum {STANdard | MONochrome}

Query Syntax

:DISPlay:GSSPectrum?

Query Response

{STANdard | MONochrome}

Description

Selects the colors used to present Gray Scale persistence waveforms. To select the gray-scale persistence mode, use the :DISPlay:PERSistence:WAVeform command for waveforms or the :DISPlay:PERSistence:EYE command for real-time eye diagrams. The following pictures show the available color schemes that you can select. The STANDard selection shows the waveform in the color selected using the :CHANnel:COLor command, the :DIFF:COLor command, or the :FUNCtion:COLor command.

Standard

Monochrome

To change the colors for color grade persistence, use the :DISPlay:CGSPectrum command.

Example Command Sequence

:DISPlay:GSSPectrum STANdard