Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:DISPlay:SKEYboard

:DISPlay General Commands
  • :DISPlay:BLAYout
  • :DISPlay:BWRap
  • :DISPlay:CGSPectrum
  • :DISPlay:CONNect
  • :DISPlay:CTHeme
  • :DISPlay:DAFFinity
  • :DISPlay:DATA?
  • :DISPlay:EXTHw:DMODe
  • :DISPlay:FMODe
  • :DISPlay:GPERformance?
  • :DISPlay:GSSPectrum
  • :DISPlay:HMToolbar
  • :DISPlay:LOCation:A{N}:AWINdow
  • :DISPlay:LOCation:A{N}:OWINdows?
  • :DISPlay:LOCation:B{N}:AWINdow
  • :DISPlay:LOCation:B{N}:OWINdows?
  • :DISPlay:LOCation:C{N}:AWINdow
  • :DISPlay:LOCation:C{N}:OWINdows?
  • :DISPlay:LOCation:D{N}:AWINdow
  • :DISPlay:LOCation:D{N}:OWINdows?
  • :DISPlay:MDISplay:DOCK
  • :DISPlay:MULTitouch:STATe
  • :DISPlay:PSIZe
  • :DISPlay:SKEYboard
  • :DISPlay:SPPanel
  • :DISPlay:SWINdows:INVert:STATe
  • :DISPlay:TOUCh:STATe
  • :DISPlay:UISCaling
  • :DISPlay:VKSignal
  • :DISPlay:WINTensity
  • :DISPlay:ZOOM
  • :DISPlay:ZOOM:SOURce

Command Syntax

:DISPlay:SKEYboard {ON | OFF | 1 | 0}

Query Syntax

:DISPlay:SKEYboard?

Query Response

{1 | 0}

Description

Turns on and off the display of the pop-up keyboard whenever data entry is required in a dialog field. Use this feature when using Infiniium 2026 that is running on a real-time oscilloscope without a keyboard connected.