:DISPlay:LOCation:A{N}:AWINdow

Command Syntax

:DISPlay:LOCation:AN:AWINdow {NONE | TIME(1:4} | DBHertz(1:4} | DHERtz(1:4}
   | SHERtz(1:4} | IRESponse(1:4} | SRESponse(1:4} | PROTocol(1:4} | RESults
   | DOUTput | MTESt(1:16} | MARKers | HRESults{1:4} | MHIStogram(1:4}
   | JITTer(1:4} | NOISe(1:4} | FPResults(1:64} | PNOise | PNMWindow
   | LLTResults | ECResults}

Where N identifies the A1, A2, A3, or A4 column in the A row of the panel location grid. For example, A1.

Query Syntax

:DISPlay:LOCation:AN:AWINdow?

Query Response

{NONE | TIME(1:4} | DBH(1:4} | DHER(1:4}
   | SHER(1:4} | IRES(1:4} | SRES(1:4} | PROT(1:4} | RES | DOUT
   | MTES(1:16} | MARK | HRES{1:4} | MHIS(1:4} | JITT(1:4}
   | NOIS(1:4}	| FPR(1:64} | PNO | PNMW | LLTR | ECR}

Description

Selects the active content window tab, results tab, or other type of tab that resides in the specified panel grid location. This command has no effect if the tab is not displayed. For example, consider if Waveform and Degrees (Hz) tabs are displayed in the window but the Markers tab is not. If you send this command with the MARKers argument, no action is taken and the message "Primary Active Window entry was not a valid selection" is displayed. The query form of this command returns the currently displayed tab.

Use the :DISPlay:LOCation:A{N}:OWINdows? command to get a list of the content windows currently assigned to the panel grid location.

The command arguments are described in the following table.

Command Argument Versus Selected Content Window
Argument Selected Content Window
TIME{1:4} Waveform 1 through 4.
DBHertz{1:4} Decibels (Hz) 1 through 4. Show the output of an FFT function with a display set to dBV or dBm.
DHERtz{1:4} Degrees (Hz) 1 through 4. Show the output of an FFT function with a display set to Phase.
SHERtz{1:4} Seconds (Hz) 1 through 4. Show the output of an FFT function with a display set to Group Delay.
IRESponse{1:4} Impulse Response 1 through 4. Added by the S-Parameter/Transfer Function Viewer.
SRESponse{1:4} Step Response 1 through 4. Added by the S-Parameter/Transfer Function Viewer.
PROTocol{1:4} Protocol 1 through 4. Added by setting up protocol decodes.
RESults Results window for measurement results.
DOUTput Reserved for future use.
MTESt{1:16} Mask Test 1 through 4 for added mask test results.
MARKers Markers window for markers results.
HRESults{1:4} W-Hist Stats 1 through 4 for waveform histogram statistics.
MHIStogram{1:4} Meas Hist N 1 through 4 for the measurement histogram statistics and plot.
JITTer{1:4} Jitter 1 through 4 for jitter measurement results and plots.
NOISe{1:4} Noise 1 through 4 for noise measurement results and plots.
FPResults{1:64} FFT Peaks 1 through 64 for FFT peak detection results.
PNOise Phase Noise analysis results.
PNMWindow Phase Noise Markers results.
LLTResults Limit Lines test results.
ECResults Eye Contours results.