:DISPlay:SWINdows:INVert:STATe
Command Syntax
:DISPlay:SWINdows:INVert:STATe {ON | OFF}
Query Syntax
:DISPlay:SWINdows:INVert:STATe?
Description
Turns on and off the inversion of the background color on all windows that display signals. When the setting is OFF, the background color is black. When the setting is ON, the background color is white. When ON, the background on saved screen images (:DISK:SIMage:SAVE) is also inverted. The command affects the following items:
- Waveform graticules
- Charts
- Screen captures