:DISPlay:ZOOM:SOURce

Command Syntax

:DISPlay:ZOOM:SOURce {CHANnel{N} | DIFF{1:4} | WMEMory{1:8}}

{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:DISPlay:ZOOM:SOURce?

Description

When the user interface Zoom Display is ON (see :DISPlay:ZOOM), this command specifies the waveform source that appears in the Zoom Display.