:DISPlay:CTHeme
Command Syntax
:DISPlay:CTHeme {"Dark Theme" | "Light Theme"}
Query Syntax
:DISPlay:CTHeme?
Description
Selects a user-interface theme that affects the look of Infiniium 2026's window and dialog boxes. The placing of double or single quotes around the string argument is required. "Dark Theme"is the Factory Default theme. A Default Setup does not change the selected theme.
This command supports the DEFault common child command.