:DISPlay:DATA?
Query Syntax
:DISPlay:DATA? [<type>[,<screen_mode>[,<compression> [,<inversion>]]]]
Description
The :DISPlay:DATA? query returns a screen capture of the Infiniium 2026 user interface.
<type> The bitmap type can be: BMP | JPG | GIF | TIF | PNG.
<screen_mode> The display setting can be: SCReen | GRATicule. Selecting GRATicule displays a 10-by-8 (unit) display graticule on the screen.
<compression> The file compression feature can be: ON | OFF. File compression is used only when the TIF bitmap type is selected.
<inversion> The inversion of the display theme: NORMal | INVert.
If no options to the query are specified, the default selections are PNG file type, SCReen mode, compression turned ON, and inversion set to NORMal.
Query Response
<binary_block _data>
Data in the IEEE 488.2 definite block format. See Definite-Length Block Response Data.