:DISPlay:VKSignal
Command Syntax
:DISPlay:VKSignal {CHANnel{N} | DIFF{1:4} | FUNCtion{1:64} | WMEMory{1:8}}
{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:DISPlay:VKSignal?
Description
When running Infiniium embedded on an oscilloscope, selects a displayed channel, differential signal, function, or waveform memory as the focus of the front-panel vertical scale knob.