:FUNCtion:PARameters:FFT:AIMPedance
Command Syntax
:FUNCtionN:PARameters:FFT:AIMPedance {ON | OFF | 1 | 0}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:FFT:AIMPedance?
Query Response
{1 | 0}
Description
For an FFT operator (see :FUNCtion:FOPerator), this command turns on or off the Auto Reference Impedance. When off, you can specify the reference impedance with the :FUNCtion:PARameters:FFT:RIMPedance command.