:FUNCtion:PARameters:FFT:PEAK:EXCursion:LEVel
Command Syntax
:FUNCtionN:PARameters:FFT:PEAK:EXCursion:LEVel <value>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
<value> is a double.
Query Syntax
:FUNCtionN:PARameters:FFT:PEAK:EXCursion:LEVel?
Description
When FFT Peak Detection is enabled (see :FUNCtion:PARameters:FFT:PEAK:ENABle), this command specifies the amplitude above the FFT waveform's noise floor necessary to be recognized as a peak.
The value is in the units selected by the :FUNCtion:PARameters:FFT:DISPlay command.