Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:FUNCtion:PARameters:FFT:PREFerence:TORigin

FFT Parameters Commands
  • :FUNCtion:PARameters:FFT:AIMPedance
  • :FUNCtion:PARameters:FFT:DETector:COUNt
  • :FUNCtion:PARameters:FFT:DETector:TYPE
  • :FUNCtion:PARameters:FFT:DISPlay
  • :FUNCtion:PARameters:FFT:NFRequency
  • :FUNCtion:PARameters:FFT:PEAK:ASCii:FDATa?
  • :FUNCtion:PARameters:FFT:PEAK:ASCii:MDATa?
  • :FUNCtion:PARameters:FFT:PEAK:COUNt
  • :FUNCtion:PARameters:FFT:PEAK:DOUBle:FDATa?
  • :FUNCtion:PARameters:FFT:PEAK:DOUBle:MDATa?
  • :FUNCtion:PARameters:FFT:PEAK:ENABle
  • :FUNCtion:PARameters:FFT:PEAK:EXCursion:LEVel
  • :FUNCtion:PARameters:FFT:PEAK:LEVel
  • :FUNCtion:PARameters:FFT:PEAK:SORT
  • :FUNCtion:PARameters:FFT:PREFerence
  • :FUNCtion:PARameters:FFT:PREFerence:TORigin
  • :FUNCtion:PARameters:FFT:RBANdwidth?
  • :FUNCtion:PARameters:FFT:RIMPedance
  • :FUNCtion:PARameters:FFT:TFACtor
  • :FUNCtion:PARameters:FFT:WINDow

Command Syntax

:FUNCtion:PARameters:FFT:PREFerence:TORigin <seconds>

<seconds> is a double.

Query Syntax

:FUNCtion:PARameters:FFT:PREFerence:TORigin?

Description

When the FFT phase reference has been set to MANual using the :FUNCtion:PARameters:FFT:PREFerence parent command, use this command to set the FFT's origin in seconds.

Parent Command

  • :FUNCtion:PARameters:FFT:PREFerence