Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:FUNCtion:PARameters:FFT:PREFerence

FFT Parameters Commands
  • :FUNCtion:PARameters:FFT:AIMPedance
  • :FUNCtion:PARameters:FFT:DETector:COUNt
  • :FUNCtion:PARameters:FFT:DETector:TYPE
  • :FUNCtion:PARameters:FFT:DISPlay
  • :FUNCtion:PARameters:FFT:NFRequency
  • :FUNCtion:PARameters:FFT:PEAK:ASCii:FDATa?
  • :FUNCtion:PARameters:FFT:PEAK:ASCii:MDATa?
  • :FUNCtion:PARameters:FFT:PEAK:COUNt
  • :FUNCtion:PARameters:FFT:PEAK:DOUBle:FDATa?
  • :FUNCtion:PARameters:FFT:PEAK:DOUBle:MDATa?
  • :FUNCtion:PARameters:FFT:PEAK:ENABle
  • :FUNCtion:PARameters:FFT:PEAK:EXCursion:LEVel
  • :FUNCtion:PARameters:FFT:PEAK:LEVel
  • :FUNCtion:PARameters:FFT:PEAK:SORT
  • :FUNCtion:PARameters:FFT:PREFerence
  • :FUNCtion:PARameters:FFT:PREFerence:TORigin
  • :FUNCtion:PARameters:FFT:RBANdwidth?
  • :FUNCtion:PARameters:FFT:RIMPedance
  • :FUNCtion:PARameters:FFT:TFACtor
  • :FUNCtion:PARameters:FFT:WINDow

Command Syntax

:FUNCtion:PARameters:FFT:PREFerence {LEFT | CENTer | MANual}

Query Syntax

:FUNCtion:PARameters:FFT:PREFerence?

Description

When the FFT output has been defined as phase, unwrapped phase, or group delay (:FUNCtion:PARameters:FFT:DISPlay command), use this command to set the FFT phase reference to LEFT, CENTer, or MANual. When MANual is specified, use the :FUNCtion:PARameters:FFT:PREFerence:TORigin command to set the FFT origin in seconds.

Child Commands

  • :FUNCtion:PARameters:FFT:PREFerence:TORigin