:FUNCtion:PARameters:FFT:PEAK:ENABle

Command Syntax

:FUNCtionN:PARameters:FFT:PEAK:ENABle {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:FFT:PEAK:ENABle?

Query Response

{1 | 0}

Description

For an FFT operator (see :FUNCtion:FOPerator), this command turns on or off the Peak Detection feature.

When on, the first N peaks in the FFT above the level specified by the :FUNCtion:PARameters:FFT:PEAK:LEVel) command are annotated.

N is specified by the :FUNCtion:PARameters:FFT:PEAK:COUNt command.

Peaks are ordered according to the :FUNCtion:PARameters:FFT:PEAK:SORT command.