:FUNCtion:PARameters:FFT:PEAK:ASCii:FDATa?
Query Syntax
:FUNCtionN:PARameters:FFT:PEAK:ASCii:FDATa?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the FFT peak frequency values as ASCII comma-separated values.
The data is sent in the order in which peaks are sorted (see :FUNCtion:PARameters:FFT:PEAK:SORT).
Use the :FUNCtion:PARameters:FFT:PEAK:COUNt command to set or query the number of annotated peaks (and values returned).
Use the :FUNCtion:PARameters:FFT:PEAK:DOUBle:FDATa? query to return the FFT peak frequency values in double format.
To get the FFT peak magnitude values, use :FUNCtion:PARameters:FFT:PEAK:DOUBle:MDATa? or :FUNCtion:PARameters:FFT:PEAK:ASCii:MDATa?.