:FUNCtion:PARameters:FFT:PEAK:COUNt
Command Syntax
:FUNCtionN:PARameters:FFT:PEAK:COUNt <number_of_peaks>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
<number_of_peaks> is an integer from 1 to 25.
Query Syntax
:FUNCtionN:PARameters:FFT:PEAK:COUNt?
Description
When FFT Peak Detection is enabled (see :FUNCtion:PARameters:FFT:PEAK:ENABle), this command specifies the number of peaks in the FFT to annotate.