:FUNCtion:PARameters:FFT:WINDow

Command Syntax

:FUNCtion{1:64}:PARameters:FFT:WINDow {RECTangular | HANNing | FTOP | BHARris | HAMMing}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:FFT:WINDow?

Description

Selects the shaping window to an FFT operator (:FUNCtion:FOPerator). You can select from Rectangular, Hanning, Flat Top, Blackman-Harris, or Hamming.

Example Command Sequence

:FUNCtion2:FOPerator FFT
:FUNCtion2:PARameters:FFT:DISPlay DBM
:FUNCtion2:PARameters:FFT:WINDow HANNing
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.