:FUNCtion:PARameters:FFT:PEAK:SORT
Command Syntax
:FUNCtionN:PARameters:FFT:PEAK:SORT {DMAG | IFReq | DFReq | IMAG}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:FFT:PEAK:SORT?
Description
When FFT Peak Detection is enabled (see :FUNCtion:PARameters:FFT:PEAK:ENABle), this command specifies the order in which peaks are sorted:
DMAG— decreasing magnitudeIFReq— increasing frequencyDFReq— decreasing frequencyIMAG— increasing magnitude