:FUNCtion:PARameters:FFT:PEAK:LEVel

Command Syntax

:FUNCtionN:PARameters:FFT:PEAK:LEVel <value>

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

<value> is a double.

Query Syntax

:FUNCtionN:PARameters:FFT:PEAK:LEVel?

Description

When FFT Peak Detection is enabled (see :FUNCtion:PARameters:FFT:PEAK:ENABle), this command specifies the level above which peaks are identified.

The value is in the units selected by the :FUNCtion:PARameters:FFT:DISPlay command.