:FUNCtion:PARameters:FFT:DETector:COUNt
Command Syntax
:FUNCtionN:PARameters:FFT:DETector:COUNt <detector_points>
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
<detector_points> is an integer from 10 to 100000 or the number of points displayed, whichever is smaller.
Query Syntax
:FUNCtionN:PARameters:FFT:DETector:COUNt?
Description
When FFT Detector Points are enabled (see :FUNCtion:PARameters:FFT:DETector:TYPE), this command specifies the maximum number of points (buckets) that detectors should decimate to.