File

With Infiniium, you can save many different types of information as shown in the table in this topic. Click the links in the table to discover how to save or load specific types of data files. Files saved within Infiniium are saved to a default subfolders located in the user data folder.

Remember to always copy important settings and waveforms to an external memory device. If your original files are damaged or lost, you can restore the files from the backup.

Back up your user files to prevent accidental loss of important data.

Saving a file … Loading a file …
Save dialog box …
Screen image file —
Setup file Choose File > Open Setup... or File > (from list of recent setup files). See Open Setup Files.
Waveform file Waveform file into memory
Color-Grade/Gray Scale CG/GS file into memory
Dedicated dialog boxes …
Documentation wizard file —
— Eye mask test file
— De-embedding network setup files
Limit line test files Limit line test file into editor
Limit test summary files —
S-Parameter data files Touchstone files (Loaded info Functions' s2p and s4p operators)
User measurement files —
SCPI recorder files SCPI recorder files