| Meas Class | Measurement Name | Description | 
			
				| "Standard" | "S11", 
				 "S21", and 
				 so forth "A_1","A_2", 
				 and so forth | S-parameter 
				 name Unratioed parameter names with notation: "receiver_source 
				 port" See Balanced 
				 S-parameter measurement names | 
			|  |  |  | 
			|  |  |  | 
			
				| "Scalar 
				 Mixer/Converter" | For input 
				 port X and output port Y: "SCXY" "SCYX" "SXX" "SYY" "Ipwr" "RevIPwr" "Opwr" "RevOPwr" | Learn 
				 about SMC parameters Note: 
				 Input and output ports are set up using the Mixer 
				 Setup dialog. If the ports are not set up using the 
				 Mixer Setup dialog, then ports 1 and 2 are the default 
				 input and output ports and the only ports that can be 
				 used. | 
			
				| "Gain 
				 Compression" Learn 
				 more "Gain 
				 Compression Converters" Learn 
				 more | GCA : | 
			
				| "CompIn21" | Input 
				 power at the compression point. | 
			
				| "CompOut21" | Output 
				 power at the compression point. | 
			
				| "CompGain21" | Gain at the compression point. | 
			
				| "CompS11" |  Input Match at the compression 
				 point | 
			
				| "RefS21" | Linear Gain | 
			
				| "DeltaGain21" | CompGain21 -Linear Gain | 
			
				| "S11", 
				 "S21", "S12", "S22" | Standard 
				 S-parameters; measured at port 1 and port 2 | 
			
				| GCX 
				 - All Gain Compression parameters (except S21 and S12) 
				 plus the following: | 
			
				| "S11" "SC21" "SC12" "S22" "Ipwr" "RevIPwr" "Opwr" "RevOPwr" | Mixer parameters | 
			
				| "Modulation Distortion" Learn 
				 more | Modulation Distortion: | 
			
				| "PIn1" | Power 
				 In | 
			
				| "POut1" | Reflected 
				 Power In | 
			
				| "POut2" | Power 
				 Out | 
			
				| "PModFile" | Power 
				 of modulation file | 
			
				| "MSig2" | Modulation 
				 Signal Out | 
			
				| "MDist2" | Modulation 
				 Distortion Out | 
			
				| "MDistIR2" | Modulation 
				 Distortion Input-referred | 
			
				| "MGain21" | Modulation 
				 Gain | 
			
				| "MComp21" | Modulation Compression | 
			
				| "PGain21" | Power Gain | 
			
				| "LMatch2" | Load match of VNA port | 
			
				| "CarrIn1" | Input Band Power | 
			
				| "CarrOut2" | Output Band Power | 
			
				| "CarrGain21" | Band Power Gain | 
			
				| "NPRIn1" | NPR at Input | 
			
				| "NPROut2" | NPR at Output | 
			
				| "NPRDist21" | NPR Distortion, Added by DUT | 
			
				| "NPRPwrIn1" | NPR Input Power | 
			
				| "NPRPwrOut2" | NPR Output Power | 
			
				| "ACPIn1" | ACP at input | 
			
				| "ACPOut2" | ACP at output | 
			
				| "ACPDist21" | ACP distortion, Added by DUT | 
			
				| "ACPPwrIn1" | ACP Input Power | 
			
				| "ACPPwrOut2" | ACP Output Power | 
			
				| "EVMDistEq21" | EVM Equalized Distortion, 
				 Added by DUT | 
			
				| "EVMDistUn21" | EVM Unequalized Distortion, 
				 Added by DUT | 
			
				| "EVMPwrIn1" | EVM Input Power | 
			
				| "EVMPwrOut2" | EVM Output Power | 
			
				| "ModFilter" | Measurement Modulation Filter | 
			
				| "A", 
				 "b1" | Port 1 test port receiver | 
			
				| "B", 
				 "b2" | Port 2 test port receiver | 
			
				| "C", 
				 "b3" | Port 3 test port receiver | 
			
				| "D", 
				 "b4" | Port 4 test port receiver | 
			
				| "R1", 
				 "a1" | Port 1 reference receiver | 
			
				| "R2", 
				 "a2" | Port 2 reference receiver | 
			
				| "R3", 
				 "a3" | Port 3 reference receiver | 
			
				| "R4", 
				 "a4" | Port 4 reference receiver | 
			|  | 
			
				| "S11" | Linear Input Match | 
			
				| "S21" | Linear Gain | 
			
				| "LPIn1" | Linear Input Match | 
			
				| "LPOut1" | Linear Reflected Power In | 
			
				| "LPOut2" | Linear Power Out | 
			
				| "Noise 
				 Figure Cold Source" Learn 
				 more | Noise 
				 Figure : | 
			
				| "NF" | Noise figure | 
			
				| "ENR" | Validate noise source 
				 measurements. | 
			
				| "T-Eff" | Effective noise temperature. | 
			
				| "DUTRNP" "DUTRNPI" | DUT noise power ratio. 
				 (Noise power expressed in Kelvin divided by 290). | 
			
				| "SYSRNP" "SYSRNPI" | System noise power ratio | 
			
				| "DUTNPD" "DUTNPDI" | DUT noise power density. 
				 (Noise power expressed in dBm/Hz). | 
			
				| "SYSNPD" "SYSNPDI" | System noise power density. 
				   | 
			
				| "OvrRng"(Opt 029 Only)
 | Indication that the noise 
				 receiver is being over powered. | 
			
				| "T-Rcvr" (Opt 
				 029 Only) | Temperature reading (in 
				 Kelvin) of the noise receiver board. | 
			|  | 
			
				| "S11", 
				 "S21", "S12", "S22" | Standard S-parameters; 
				 measured with the port1 and port2 noise switches set for 
				 noise mode. | 
			
				| "A_1","A_2" 
				 ...and so forth. | Unratioed 
				 parameters; with notation:"receiver, source port"
 | 
			
				| "GammaOpt" | Optimum 
				 Complex Reflection Coefficient | 
			
				| "Rn" | Noise 
				 Resistance | 
			
				| "NFMin" | Minimum noise figure that 
				 occurs at GammaOpt | 
			|  | 
			|  |  | 
			|  |  | 
			|  |  | 
			
			
			
			
			
			
			
			
			
			
			
			
				| "Differential 
				 I/Q" Learn 
				 more | Create custom parameters 
				 using Sens:DIQ:Par:Def, 
				 then specify your custom parameter name here. The following are default parameters: | 
			
				| "IPwrF1" "OPwrF1" "GainF1" | Input Power over F1 range Output Power over F1 range Gain over F1 range | 
			
				| "Spectrum 
				 Analyzer" Learn 
				 more | "a<n>" "b<n>" where 
				 <n> is the 
				 port number to measure "ImageReject<n>" where 
				 <n> is the image reject trace | Reference 
				 receiver Test port receiver |