:CHANnel:PATTern:FILE:GCODe
Command Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:FILE:GCODe {ON | OFF}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
Query Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:FILE:GCODe?
Description
Indicates if the PAM pattern waveform file that has been imported into associated with a specific waveform signal processing function uses gray coding. on the Turns gray coding on or off for PAM waveforms. When a pattern file is imported into FlexDCA ( :CHANnel:PATTern:MODE command), the imported file may use gray coding. Use this command to indicate the use of gray coding. Be sure to use the :CHANnel:PATTern:FORMat command first to specify a PAM formatted waveform.
Turns gray coding on or off for PAM waveforms. When a pattern file is imported into FlexDCA ( :CHANnel:PATTern:MODE command), the imported file may use gray coding. Use this command to indicate the use of gray coding. Be sure to use the :CHANnel:PATTern:FORMat command first to specify a PAM formatted waveform.
ON- The pattern file uses gray coding.
OFF- The pattern file does not uses gray coding.
Gray coding, or reflected binary code, is a coding pattern where successive symbols differ by one binary bit which reduces errors in high speed waveforms. For example in the case of PAM4, decimal 0, 1, 2, and 3 is expressed in gray coding as 00, 01,11, and 10.
When a chain of multiple functions is configured and the Output Pattern Symbol Sequence settings Output Tracks Input is on, the following occurs. If you change the pattern symbol sequence on any function in the chain as well as the input waveform (channel, differential, or waveform memory) the setting is changed on all other functions in the chain as well as the input waveform.
Requires FlexDCA revision A.08.40 or greater.
Example Command
:CHANnel2A:PATTern:FILE:GCODe ON