:CHANnel:PATTern:FILE:RELoad

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:CHANnel{1:8}{A|B|C|D}:PATTern:FILE:RELoad

Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).

Description

Reloads a BERT pattern file (*.ptrn) that has previously been loaded using the :CHANnel:PATTern:FILE:NAMe command.

When a chain of multiple functions is configured and the Output Pattern Symbol Sequence settings Output Tracks Input is on, the following occurs. If you change the pattern symbol sequence on any function in the chain as well as the input waveform (channel, differential, or waveform memory) the setting is changed on all other functions in the chain as well as the input waveform.

Requires FlexDCA revision A.08.40 or greater.

Example Command

:CHANnel2A:PATTern:FILE:RELoad