:CHANnel:PATTern:TRACking
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:TRACking {OFF}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
Query Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:TRACking?
Description
For channels, tracking of the waveform's Pattern Symbol Sequence is always off so the sending of this command has no effect. The query for of the command always returns a "0" for off and automatic detection of the pattern is selected (:CHANnel1A:PATTern:MODE). You can turn off automatic detections and use the remaining commands shown in this topic's sidebar to specify the format and pattern.
Requires FlexDCA revision A.08.40 or greater.
Example Command
:CHANnel2B:PATTern:TRACking?