:CHANnel:PATTern:FORMat
Command Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:FORMat {PAM4}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
Query Syntax
:CHANnel{1:8}{A|B|C|D}:PATTern:FORMat?
Description
Specifies the format of the waveform that is input to the equalizer: PAM4. You would use this command whenever you have turned off automatic detection of the waveform's Pattern Symbol Sequence with the :CHANnel:PATTern:MODE command.
When a chain of multiple functions is configured and the Output Pattern Symbol Sequence settings Output Tracks Input is on, the following occurs. If you change the pattern symbol sequence on any function in the chain as well as the input waveform (channel, differential, or waveform memory) the setting is changed on all other functions in the chain as well as the input waveform.
Requires FlexDCA revision A.08.40 or greater.
Example Command
:CHANnel2B:PATTern:FORMat PAM4