:CHANnel:PATTern:MODE

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:CHANnel{1:8}{A|B|C|D}:PATTern:MODE  {AUTodetect | KPATtern | PFILe}

Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).

Query Syntax

:CHANnel{1:8}{A|B|C|D}:PATTern:MODE?

Description

Selects the method used to specify the input signal waveform's pattern symbol sequence that is input to the equalizer. The arguments are:

AUTodetect
The function automatically detects the waveform's pattern symbol sequence. This is the default setting.
KPATtern
Specifies a known pattern symbol sequence using the following commands. The ":CHANnel:PATTern:FORMat command is used to specify an NRZ or PAM4 pattern. The CHANnel:PATTern:KPATtern command is used to specify the actual pattern.
PFILe
Selects a pattern file. Use the ":CHANnel:PATTern:FILE:NAMe command to enter the name of the pattern file. You can also reload a pattern file using the ":CHANnel:PATTern:FILE:RELoad command. Use the :CHANnel:PATTern:FORMat command to specify an NRZ or PAM4 pattern. If a PAM4 format is selected, use the ":CHANnel:PATTern:FILE:GCODe command to indicate if the pattern file uses gray coding.

By default, the equalizer automatically detects the input waveform's pattern symbol sequence. However, you can use this command to select a Known Pattern of type NRZ or PAM4 or you can load a specific Pattern File.

When a chain of multiple functions is configured and the Output Pattern Symbol Sequence settings Output Tracks Input is on, the following occurs. If you change the pattern symbol sequence on any function in the chain as well as the input waveform (channel, differential, or waveform memory) the setting is changed on all other functions in the chain as well as the input waveform.

Requires FlexDCA revision A.08.40 or greater.

Example Command

:CHANnel2B:PATTern:MODE AUTodetect