:CHANnel:PATTern:FILE:NAME

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:CHANnel{1:8}{A|B|C|D}:PATTern:FILE:NAME <file name>

Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).

Where <file name> is the name, including path, to a pattern file.

Query Syntax

:CHANnel{1:8}{A|B|C|D}:PATTern:FILE:NAME?

Description

Uploads a BERT pattern file (*.ptrn) to a specified waveform signal processing function. Before sending this command, send the :CHANnel:PATTern:MODE command to turn autodetection of the Pattern Symbol Sequence off and select that a pattern file be uploaded instead. If the name of the pattern file has previously been entered (as returned by the query form of this command), you can use the :CHANnel:PATTern:FILE:RELoad command instead.

When a chain of multiple functions is configured and the Output Pattern Symbol Sequence settings Output Tracks Input is on, the following occurs. If you change the pattern symbol sequence on any function in the chain as well as the input waveform (channel, differential, or waveform memory) the setting is changed on all other functions in the chain as well as the input waveform.

Requires FlexDCA revision A.08.40 or greater.

Example Command

:CHANnel2B:PATTern:FILE:NAME "C:\Documents\Keysight\FlexDCA\Patterns\test-pattern.ptrn"