:CHANnel:SCRecovery:DEMethod
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:DEMethod {CCRossing | PCRossings}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:DEMethod?
Description
For the selected channel, selects the edge detection method that is applied to the software clock recovery. You can select an edge detection of either Center Crossing (CCRossing) or PAM4 Crossings (PCRossings), which is the default setting.
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:SCRecovery:DEMethod PCRossings