:CHANnel:SCRecovery:PLLoop:ORDer
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:PLLoop:ORDer {FIRSt | SECond | THIRd}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:PLLoop:ORDer?
Query Response
{FIRS | SEC | THIR}
Description
For the selected channel's software clock recovery, selects a first, second, or third order low-pass filter for the FlexRT software clock recovery's phase lock loop. The following arguments are used:
- FIRSt
- Selects a first-order loop. Use the
:CHANnel:SCRecovery:PLLoop:MODEcommand to define either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) type of PLL. The transfer functions are defined using the:CHANnel:SCRecovery:PLLoop:JTF:BANDwidthand:CHANnel:SCRecovery:PLLoop:OJTF:BANDwidthcommands. - SECond
- Selects a second-order loop. This is the default selection. Use the
:CHANnel:SCRecovery:PLLoop:MODEcommand to define either the Jitter Transfer Function (JTF) or Observed Jitter Transfer Function (OJTF) type of PLL. The JTF is defined using the:CHANnel:SCRecovery:PLLoop:JTF:BANDwidthand:CHANnel:SCRecovery:PLLoop:JTF:PEAKingcommands. The OJTF is defined using the:CHANnel:SCRecovery:PLLoop:OJTF:BANDwidthand:CHANnel:SCRecovery:PLLoop:OJTF:DFACtorcommands. - THIRd
- Selects a third-order loop. Use the
:CHANnel:SCRecovery:PLLoop:FGAIncommand to enter the frequency for the loop's gain. Use the:CHANnel:SCRecovery:PLLoop:FPOLecommand to enter the frequency for the loop's pole. Use the:CHANnel:SCRecovery:PLLoop:FZERocommand to enter the frequency for the loop's zero.
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:SCRecovery:PLLoop:ORDer FIRSt