:CHANnel:SCRecovery:STATe
Command Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:STATe {ON | OFF}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:SCRecovery:STATe?
Description
For the selected channel, turns the application of FlexRT software clock recovery ON or OFF. Software clock recovery is applied to the UXR-series oscilloscope's input waveform. The default setting for software clock recovery is on.
Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:SCRecovery:STATe ON