:CHANnel:SCRecovery:PLLoop:JTF:BANDwidth

Instrument:
UXR Scope
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:CHANnel{1:8}{A|B|C|D}:SCRecovery:PLLoop:JTF:BANDwidth <bandwidth>

<bandwidth> is a double.

Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).

The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.

Query Syntax

:CHANnel{1:8}{A|B|C|D}:SCRecovery:PLLoop:JTF:BANDwidth?

Description

For the selected channel's software clock recovery, defines the bandwidth of a first- or second-order PLL's Jitter Transfer Function (JTF). The following table shows the bandwidth settings for some standards. Use the :CHANnel:SCRecovery:PLLoop:OJTF:BANDwidth command to set the bandwidth of the Observed Jitter Transfer Function (OJTF).

Standard JTF Bandwidth Settings
Standard First-Order Loop Filter Second-Order Loop Filter
SAS 1.5 Gb/s 900.0 kHz 900.0 kHz
SAS-SSC 1.5 Gb/s — 2.328 MHz
SATA 1.5 Gb/s — 4.097 MHz
SAS 3.0 Gb/s 1.800 MHz 1.800 MHz
SAS-SSC 3.0 Gb/s — 3.291 MHz
SATA 3.0 Gb/s — 1.791 MHz
SAS 6.0 Gb/s 3.600 MHz 3.600 MHz
SAS-SSC 6.0 Gb/s — 4.655 MHz
SATA 6.0 Gb/s — 8.194 MHz
QPI — 5.692 MHz
USB 3.0 — 10.03 MHz

Before this command can take effect, you must disable shared acquisition parameters with the :CHANnel:RTSCope:TRACkcommand.

Requires FlexDCA revision A.06.70 and above.

Example Command

:CHANnel2A:SCRecovery:PLLoop:JTF:BANDwidth 4.0E+6