:CRECovery:JSANalysis:OPTimize:EMBedded

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Command Syntax

:CRECovery{1:8}:JSANalysis:OPTimize:EMBedded

Where the {1:8} specifier identifies a slot number. The slot number is associated with the N1060A, N1076A/B, N1077A, N1078A, or 86108B module with Option JSA. When an 86108B module is used, the slot number is always 1.

Description

Optimizes a JSA spectrum that is selected to be the EMULated with the :CRECovery:JSANalysis:SPECtrum command. After configuring the Clock Recovery Emulation PLL, use this command to obtain the optimum CRE spectrum fidelity. This command automatically sets, as closely as possible, the hardware CDR parameters to the CRE PLL settings. You can manually configure these settings using the :CRECovery:CLBandwidth and :CRECovery:LSELect commands.

Requires FlexDCA revision A.01.70 and above.

Requires a clock-recovery module that has Option JSA (Jitter Spectrum Analysis and SW Clock Recovery Emulation).

Command Compatibility

  • N1060A Option JSA
  • 86108A/B Option JSA
  • N107X-series Option JSA

Example Command Sequence

:CRECovery{1:8}:JSANalysis:OPTimize:EMBedded